SC18IS604PWJ Thermal Values

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SC18IS604PWJ Thermal Values

ソリューションへジャンプ
1,450件の閲覧回数
canton
Contributor II

Dear Mr/Mrs,

I woud like to know the following characteristics of the SC18IS604PWJ component:

Temperature Junction maximum.
Thermal Rj-c
Thermal Rj-b

Thanks in advance,

Best regards,

Carlos Antón

0 件の賞賛
返信
1 解決策
1,384件の閲覧回数
giraffe508
Contributor IV

Hi Carlos,

The thermal values for the SC18IS604PWJ component from our Package team. Here are the values:

  • Temperature Junction maximum (Tj-max): 150°C
  • Thermal Resistance Junction-to-Ambient (Rj-a): 130°C/W
  • Thermal Resistance Junction-to-Case (Rj-c): 40°C/W
  • Thermal Resistance Junction-to-Board (Rj-b): 20°C/W

Please note that these values are typical and can vary depending on the specific application and PCB design. For more information on the SC18IS604PWJ component, you can refer to the datasheet.

If you have any further questions or need assistance, please feel free to ask.

Best regards,

元の投稿で解決策を見る

5 返答(返信)
1,385件の閲覧回数
giraffe508
Contributor IV

Hi Carlos,

The thermal values for the SC18IS604PWJ component from our Package team. Here are the values:

  • Temperature Junction maximum (Tj-max): 150°C
  • Thermal Resistance Junction-to-Ambient (Rj-a): 130°C/W
  • Thermal Resistance Junction-to-Case (Rj-c): 40°C/W
  • Thermal Resistance Junction-to-Board (Rj-b): 20°C/W

Please note that these values are typical and can vary depending on the specific application and PCB design. For more information on the SC18IS604PWJ component, you can refer to the datasheet.

If you have any further questions or need assistance, please feel free to ask.

Best regards,

1,443件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Please help and fill below:

1: company name /location

2: project schedule

3: volume/annual

0 件の賞賛
返信
1,428件の閲覧回数
canton
Contributor II

Hello guoweisun,

I would also need the Rj-a resistor value of the component. So as a sumarize:

  1. Temperature Junction maximum.
  2. Thermal Rj-a
  3. Thermal Rj-c
  4. Thermal Rj-b

Sorry for the inconvenience,

Best regards,

Carlos

0 件の賞賛
返信
1,441件の閲覧回数
canton
Contributor II

Dear guoweisun

1: company name /location: Tecnobit, Madrid

2: project schedule: Design stage

3: volume/annual: up to 660 units

 

0 件の賞賛
返信
1,390件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Carlos,

Please accept our apologies for the delay in getting back to you, we currently do not have the required thermal values, but working on it and will update this thread as soon as I get them from our Package team.

Best regards,

Tomas

0 件の賞賛
返信