SC18IS604PWJ Thermal Values

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC18IS604PWJ Thermal Values

Jump to solution
1,054 Views
canton
Contributor II

Dear Mr/Mrs,

I woud like to know the following characteristics of the SC18IS604PWJ component:

Temperature Junction maximum.
Thermal Rj-c
Thermal Rj-b

Thanks in advance,

Best regards,

Carlos Antón

0 Kudos
Reply
1 Solution
988 Views
giraffe508
Contributor IV

Hi Carlos,

The thermal values for the SC18IS604PWJ component from our Package team. Here are the values:

  • Temperature Junction maximum (Tj-max): 150°C
  • Thermal Resistance Junction-to-Ambient (Rj-a): 130°C/W
  • Thermal Resistance Junction-to-Case (Rj-c): 40°C/W
  • Thermal Resistance Junction-to-Board (Rj-b): 20°C/W

Please note that these values are typical and can vary depending on the specific application and PCB design. For more information on the SC18IS604PWJ component, you can refer to the datasheet.

If you have any further questions or need assistance, please feel free to ask.

Best regards,

View solution in original post

5 Replies
989 Views
giraffe508
Contributor IV

Hi Carlos,

The thermal values for the SC18IS604PWJ component from our Package team. Here are the values:

  • Temperature Junction maximum (Tj-max): 150°C
  • Thermal Resistance Junction-to-Ambient (Rj-a): 130°C/W
  • Thermal Resistance Junction-to-Case (Rj-c): 40°C/W
  • Thermal Resistance Junction-to-Board (Rj-b): 20°C/W

Please note that these values are typical and can vary depending on the specific application and PCB design. For more information on the SC18IS604PWJ component, you can refer to the datasheet.

If you have any further questions or need assistance, please feel free to ask.

Best regards,

1,047 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please help and fill below:

1: company name /location

2: project schedule

3: volume/annual

0 Kudos
Reply
1,032 Views
canton
Contributor II

Hello guoweisun,

I would also need the Rj-a resistor value of the component. So as a sumarize:

  1. Temperature Junction maximum.
  2. Thermal Rj-a
  3. Thermal Rj-c
  4. Thermal Rj-b

Sorry for the inconvenience,

Best regards,

Carlos

0 Kudos
Reply
1,045 Views
canton
Contributor II

Dear guoweisun

1: company name /location: Tecnobit, Madrid

2: project schedule: Design stage

3: volume/annual: up to 660 units

 

0 Kudos
Reply
994 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Carlos,

Please accept our apologies for the delay in getting back to you, we currently do not have the required thermal values, but working on it and will update this thread as soon as I get them from our Package team.

Best regards,

Tomas

0 Kudos
Reply