Hi, all ! I want to use a SBC Controller UJA1075A in a non-automotive solution. My question is, is there a little bit software-support for this part, for example a LIB-File or an INCLUDE File for C ? Thanks. Claus
Hello everyone,
Did anyone manage to implement this SBC? Is it possible to share the code of function void SpiSend(unsigned int *tx) ?
I have some troubles to activate CAN 5V, for example I send 0x2C00 but nothing happens.
Is there any way to test if the communication is working properly?
Best.
Hello, Tomas,
Yeah! It's more, more than I expected. Thanks!
So I do not have to reinvent the bike.
I know, that such SBC's with combined LIN/LON receivers were designed especially for automotive applicaions.
It's not easy to buy it, and you must buy at least 2.000 pieces at once. this will be my annual requirements.
I hope, I can get some samples from NXP for my prototypes.
Once again: Thank You !!
Best regards,
Claus
Hi Tomas , can you help me with the software "uja 1168" or, for example, lib file or include file for C ?