SAF85XX L2 Cache Invalidation and Flush

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SAF85XX L2 Cache Invalidation and Flush

590 Views
eddy_bts
Contributor III

Cortex A53 core which is located in SAF85XX has two types of caches. L1 and L2.

Zephyr cache-related code is like:
 
#include <cache.h>
#include <syscall_handler.h>

static inline int z_vrfy_sys_cache_data_all(int op)
{
    return z_impl_sys_cache_data_all(op);
}
#include <syscalls/sys_cache_data_all_mrsh.c>

static inline int z_vrfy_sys_cache_data_range(void *addr, size_t size, int op)
{
    Z_OOPS(Z_SYSCALL_MEMORY_WRITE(addr, size));

    return z_impl_sys_cache_data_range(addr, size, op);
}
#include <syscalls/sys_cache_data_range_mrsh.c>

static inline int z_vrfy_sys_cache_instr_all(int op)
{
    return z_impl_sys_cache_instr_all(op);
}
#include <syscalls/sys_cache_instr_all_mrsh.c>

static inline int z_vrfy_sys_cache_instr_range(void *addr, size_t size, int op)
{
    Z_OOPS(Z_SYSCALL_MEMORY_WRITE(addr, size));

    return z_impl_sys_cache_instr_range(addr, size, op);
}
#include <syscalls/sys_cache_instr_range_mrsh.c>
 
APIs above is applied to L1 and L2 cache both? Otherwise only to L1 cache?
Please let me know how to flush or invalidate L2 cache.
0 Kudos
Reply
4 Replies

507 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

The [Zephyr Cache Management API](https://docs.zephyrproject.org/3.3.0/hardware/cache/index.html) is a generic API for any type of I/D caches, either implemented by the architecture, for instance, in case of L1/L2 caches available in the core itself like Cortex-A53; or implemented by a cache controller driver, for instance, in case of L2 caches externals to the core. This API can be enabled in your driver/application through [CONFIG_CACHE_MANAGEMENT](https://docs.zephyrproject.org/latest/kconfig.html#CONFIG_CACHE_MANAGEMENT)
The code you are looking for the cache management on A53, is in zephyr/arch/arm64/core/cache.c for v2.7.2 (latest SAF85xx release).
The only APIs implemented are for D-cache and operate over all the cache levels implemented in the core. When acting over all cached memory, it does it by set/way. When acting over a range of memory (VA), it does it to PoC (point of coherence, which is always outside the processor).

There’s also a chapter available in Auto Zephyr user manual, “8.2.1 Non-Cacheable section on core A53” from SW32SAF85xx_AZ_2.7.2_0.9.0_D2208__User_Manual.pdf
Zephyr allows to create a “nocache” read-write memory section configured as no-cache through [CONFIG_NOCACHE_MEMORY.](https://docs.zephyrproject.org/latest/kconfig.html#CONFIG_NOCACHE_MEMORY)

Best regards,

Peter

0 Kudos
Reply

548 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

The issue is currently being analyzed. Could you tell me which specific file the code in question comes from?

Best regards,

Peter

0 Kudos
Reply

528 Views
eddy_bts
Contributor III

zephyr/arch/arc/core/cache.c

0 Kudos
Reply

570 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I have created internal ticket for this. The RADAR team will either reply here, or I will share answer.

Best regards,

Peter

0 Kudos
Reply