Has anyone encountered this problem?
On the basis of "RSDK_Multi_RFE_example_S32R45" I tried to run 1024-512-16 range with RF and SPT ( The output data format is "CP4Q_FMTA" ) . I found it OK to put the processed data on SRAM. But if i want to put the processed data on DDR it will not succeed. Because SPT does not return the completion callback "SptEcsIsrCb". So I wonder if it is possible that the DDR speed is not as fast as the SRAM, causing the loss of chirp?
Hello,
If the issue is still relevant can you please submit a ticket at NXP.com so I can escalate this to RADAR team?
Best regards,
Peter