S32R274 cannot enter stop0 mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32R274 cannot enter stop0 mode

493件の閲覧回数
q_zhang
Contributor I

The chip S32R274 can enter run0 mode from DRUN mode successfully, but can not enter stop0 mode then.

I tried it without debugger. In DRUN mode the current is 213mA. When ithe chip tried to enter stop0 mode, the current is 155mA, which I don't think it works in stop0 mode.

1.png

0 件の賞賛
3 返答(返信)

460件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

This looks like some clock sources are active, before execution of mode transition to stop mode.

Unfortunately I do not have at Home Office this micro at this moment.

I have ordered it and as soon as it arrive I will write test code and test it.

Best regards,
Peter

0 件の賞賛

481件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Your code looks correct to me.

What happen if you execute the STOP0 mode transition.

Is it stuck at while loop waiting for MTRANS to finish) or does it pass?

Best regards,

Peter

0 件の賞賛

479件の閲覧回数
q_zhang
Contributor I

Hello,

It stucks at while loop waiting for MTRANS to finish.

0 件の賞賛