S32R274 cannot enter stop0 mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32R274 cannot enter stop0 mode

491 Views
q_zhang
Contributor I

The chip S32R274 can enter run0 mode from DRUN mode successfully, but can not enter stop0 mode then.

I tried it without debugger. In DRUN mode the current is 213mA. When ithe chip tried to enter stop0 mode, the current is 155mA, which I don't think it works in stop0 mode.

1.png

0 Kudos
3 Replies

458 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

This looks like some clock sources are active, before execution of mode transition to stop mode.

Unfortunately I do not have at Home Office this micro at this moment.

I have ordered it and as soon as it arrive I will write test code and test it.

Best regards,
Peter

0 Kudos

479 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Your code looks correct to me.

What happen if you execute the STOP0 mode transition.

Is it stuck at while loop waiting for MTRANS to finish) or does it pass?

Best regards,

Peter

0 Kudos

477 Views
q_zhang
Contributor I

Hello,

It stucks at while loop waiting for MTRANS to finish.

0 Kudos