S32 Design Studio for S32 Plaform 3.5 License Missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Studio for S32 Plaform 3.5 License Missing

367 Views
Ean
Contributor II
Open the project project with S32KDS 3.5, and it prompts that the license missing. Maybe it's because I reinstalled the system, but when I reactivated it with the license, it prompts the following error. What should I do? Reinstall the software? 1.jpg2.jpg
0 Kudos
Reply
8 Replies

356 Views
Ean
Contributor II
After uninstalling the original program and reinstalling it, I installed and activated it online using the license I received in the previous email. However, the installation failed and the following malfunctions occurred, and the installation with administrator privileges still occurred
 
20240625-165714.jpg
0 Kudos
Reply

346 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Ean 

Based on the log file looks like the installer is not able to write some files on the hard drive. It may be because of OS privileges and limitations. Are you installing the S32DS as an administrator?

 

B.R.

VaneB

0 Kudos
Reply

330 Views
Ean
Contributor II
Yes, I am running in administrator mode, and I enter the corresponding folder to run cllSvrUtilty.exe in administrator mode, but it also cannot be executed.
0 Kudos
Reply

318 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Ean 

It appears you are attempting to install S32 Design Studio 3.5 onto Windows 11. Could you please confirm this information? 

0 Kudos
Reply

297 Views
Ean
Contributor II
Yes, the computer I'm using is WINDOWS 11, but my other colleagues were able to install it successfully and consulted the company's IT department, and there were no special permission restrictions on the computer, so I'm wondering if it's because some files couldn't be deleted due to uninstallation, making it impossible to reinstall
0 Kudos
Reply

280 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Ean 

As the installation on Windows 11 is not officially supported there are some suggestions from what has been observed from customers who have successfully achieved this. You can refer to the S32DS installation error.

0 Kudos
Reply

172 Views
Ean
Contributor II
I have tried all the methods inside, but still cannot solve the problem of installation failure
0 Kudos
Reply

168 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Ean 

Just to make sure, did you follow all the installation steps as described in the following document?

S32 Design Studio for S32 Platform Installation User Guide

0 Kudos
Reply