Dear Responsible,
I have purchased some products as listed;
BGA2714
BGA2800
BGA2803
BGA2815
BGA2817
However, I could not find their s-parameter data on web. Can you provide me with these product's s-parameter or model data?
Thanks,
Best Regards,
Naci
Daer Naci
S-parameters can be found in the Datasheets:
BGA2714 : http://cache.nxp.com/documents/data_sheet/BGA2714.pdf
BGA2800 : http://cache.nxp.com/documents/data_sheet/BGA2800.pdf
BGA2803 : http://cache.nxp.com/documents/data_sheet/BGA2803.pdf
BGA2815 : http://cache.nxp.com/documents/data_sheet/BGA2815.pdf
BGA2817 : http://cache.nxp.com/documents/data_sheet/BGA2817.pdf
Best regards
Andrei
Dear Andrei,
I have checked the datasheets before and now a couple of times. However, I need the S-Parameter data as given in the datasheet of BGA2714 in section 8.3. Other devices' datasheets contain only the graphs of the scattering parameters and values at 3 different frequencies. Those data are useless unless they are given as in the table provided in the datasheet of BGA2714 in section 8.3. I cannot derive the numbers from the graphs in with a good precision, furthermore, phases are not available in those datasheets. Can you provide me with the scattering parameters as a table for each component?
Best Regards,
Naci
All available S-parameter data can be found in the Datasheets. We don't have any additional information available.