Re: PCA9617 I2C signals getting damaged during Hot swapping/Insertion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Re: PCA9617 I2C signals getting damaged during Hot swapping/Insertion

1,260 Views
reyes
NXP TechSupport
NXP TechSupport

For hot-swapping operations, you need a device with circuitry that precharges the SDA and SCL pins to prevent glitching data on an active I2C bus when the unpowered slave card is inserted into the backplane system. Unfortunately, the PCA9617 does not include this feature, I recommend you to switch to a hot-swappable translator like the PCA9511/12/13/14 Hot Swappable I2C Buffers:
PCA9511A: https://www.nxp.com/docs/en/data-sheet/PCA9511A.pdf

PCA9512: https://www.nxp.com/docs/en/data-sheet/PCA9512A_PCA9512B.pdf

PCA9513/14: https://www.nxp.com/docs/en/data-sheet/PCA9513A_PCA9514A.pdf

0 Kudos
Reply
3 Replies

1,097 Views
vihang_vinayak
Contributor II

Dear Jose,

Could you let me know what level of voltage stress will the PCA9511/12/13/14 Hot Swappable I2C Buffers can tolerate during Hot swap at the I2C pins on them?

Appreciate your reply.

0 Kudos
Reply

1,097 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

Limiting values on I2C pins is +7V.

 

Regards,

Jose

NXP Semiconductors

0 Kudos
Reply

1,097 Views
vihang_vinayak
Contributor II

Dear Jose,

I tested with PCA9514, the hot swap is working fine. Thanks for your support

Also I am operating the PCA9514 at 5V and then I need to translate the I2C signals to 3.3V for which I used the PCA9617. I connected the PCA9514 output to Port B of PCA9617, but the interface is not working because according to the PCA9617 datasheet the Port B has static offset.

So should I connect the PCA9514 output to Port A of PCA9617, Is it valid?  

Please let me know your suggestion

Regards,

Vihang

0 Kudos
Reply