Hello all,
I am new here and still a novice when it comes to the world of RFID. I'm wondering if there is a RFID reader and key chain tag that can be read from 2-3 feet away? I want to use this in conjunction with an Arduino Uno and a couple of linear actuators to open a door when the tag is in range of the reader (2-3 feet away) and then close the door when the tag is no longer in range of the reader.
Thanks in advance for the help!
Hello,
As mentioned in case:
Hi Ivan and thanks for the reply! As I mentioned, I am VERY new to all of this, so please excuse the very basic questions. In reading through the description of those products, it does appear that they are exactly what I am looking for. However, what I don't understand is which of these products would be compatible with Arduino Uno? And if compatible, how do I integrate it with the Arduino? Do I need to solder leads to connect to the Arduino and build my own antenna? What about code to make it work with the Arduino?
Hi,
Sure, I forgot to mention the family products above are for the Tags, now you will need a reader to work with them in this Reader-Tag environment.
For ICODE, you may refer to the following reader: SLRC61003HN | NXP
For UCODE you may contact one of the reader manufacturers since NXP does not currently have readers for UCODE family: RFID Ecosystem | NXP
Hope this help.
BR,
Ivan.