In the document SMI-N2000 Advantages of Solid State RF Power Over Vacuum Tubes ,I have see an apllication of RF dielectric heating . And want to make an instrument like RFEM24-250 using for heating. ISM band is 40MHz,and the Transistor is useing MRFE6VP6300H or MRFE6VP5150N.
I want to find the reference design or technical support
MRFE6VP5150,MRFE6VP6300H can be used for 40MHz industrial heating application but unfortunately we have no 40MHz reference designs for these parts. 40MHz designs are available for MRFE6VP61K25H, MRF300AN.
Please, we can discuss possible design using MRFE6VP5150,MRFE6VP6300H or other suitable devices. The RF power range is from ten watts to 1.8kW.
Have a great day,
Pavel
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
40MHz design can be changed. Rf dielectric heating is my requirement. 6 to 41MHz designs are suitable for my using,which can heating up to 300 °C as fast as posible.
I have find a design using MRF1K50H and it`s development boards (27Mhz). but I can not understand how to use this for RF dielectric heating.
so ,first of all ,I need to heating up to 300 °C ( the speed can consider in next step ) with a designing scheme using MRF1K50H or MRFE6VP5150 and so on.
can NXP give me a reference design for industrial RF heating just as training?
Have a great day,
zhao xin