Hi all,
I met something not sure, here is the problems:
1. do I need to pull up SLP_N pin? I see the official development board pulls up it.
2. If I pull up SLP_N pin with the voltage powered on earlier than VBAT=12V, will it do harm to the chip?
Here is the circuit, VDD3V3 will power on ealier than VDD12V
Best Regards,
Yuanyuan.