Problem with MCUXpresso IDE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with MCUXpresso IDE

Jump to solution
1,790 Views
VictorPastrana
Contributor III

Hi, Im having troubles trying to load an SDK to MCUxpresso IDE, i download them from the SDK builder from NXP and i make them only for MCUxpresso IDE. But it continues to show me the error that the SDK is incorrect or that the SDK is NULL. 

Already tried different SDKs for different boards, re-install MCUxpresso and nothing seems to work. 

Could you tell me what can i do to fix this problem?

FYI im working with the 11.7.1_9221 version.

#MCUXpresso #IDE #Help

 

 

0 Kudos
Reply
1 Solution
1,777 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @VictorPastrana 

The SDK2.14 doesn't support MCUXpresso IDE v11.7, need V11.8, while the IDE v11.8 have not released, so please download SDK2.13 to use.

Detail you can have a look at below thread:

https://community.nxp.com/t5/MCUXpresso-SDK/Unable-to-find-valid-manifest-files-in-SDI-SDI-2-14-0-LP...  

Alice_Yang_0-1690854433807.png

 

BR

Alice

View solution in original post

0 Kudos
Reply
3 Replies
1,755 Views
VictorPastrana
Contributor III

Thanks a lot, Alice!!

0 Kudos
Reply
1,700 Views
Alice_Yang
NXP TechSupport
NXP TechSupport
1,778 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @VictorPastrana 

The SDK2.14 doesn't support MCUXpresso IDE v11.7, need V11.8, while the IDE v11.8 have not released, so please download SDK2.13 to use.

Detail you can have a look at below thread:

https://community.nxp.com/t5/MCUXpresso-SDK/Unable-to-find-valid-manifest-files-in-SDI-SDI-2-14-0-LP...  

Alice_Yang_0-1690854433807.png

 

BR

Alice

0 Kudos
Reply