Hello ,
I'm currently working on the TWR-LS1021A LSDK board. I need to flash both the SD Card and NOR Flash on the board. I need a proper pre-built image. I have already downloaded a Real Time Edge TWR-LS1021A-PC Image which was not the proper image. I need a proper binary without the Edge where I can boot both the SD card and NOR Image without any issue. Below I have attached the TWR-LS1021A-PC Real Time Edge Image link which I have downloaded and flashed before.
Can you please help me with a valid pre-built image.
Thanks in Advance.
Thank you for your reply @Oswalag
I tried with the image link you've shared with me its getting booted successfully. I need to work on NOR flash, But the issue is the /dev/mtd flash memory partition is not detecting.
root@OpenWrt:/# ls /dev/mtd
mtd0 mtd0ro mtdblock0
The partition I need.
root@ls1021atwr:/run/media/mmcblk0p1# flashcp uboot.bin /dev/mtd
mtab mtd1 mtd2ro mtd4 mtd5ro mtd7 mtd8ro mtdblock0 mtdblock3 mtdblock6 mtdblock9
mtd0 mtd1ro mtd3 mtd4ro mtd6 mtd7ro mtd9 mtdblock1 mtdblock4 mtdblock7
mtd0ro mtd2 mtd3ro mtd5 mtd6ro mtd8 mtd9ro mtdblock2 mtdblock5 mtdblock8
Can you please help me with an apt image for NOR flash.
Thanks in Advance.