IMX93EVK with xfs images.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX93EVK with xfs images.

115 Views
ranga_yn
Contributor III

Hello team,

currently when i build the image and flash its vfat for boot and rootfs is ext4 - can the image be supported with XFS , if yes how to do the same any steps.

imx-image-core-imx93evk.rootfs-20240504074502.wic.zst 

If the above is not possible and  want to have extra partition - of xfs will that be supported if yes , can some one guide the same

 

Thanks

R

 

0 Kudos
Reply
1 Reply

106 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

 

Yes Yocto BSP support server-side copy for CIFS, NFS, XFS, support for hard discs with host-managed SMR (Shingled Magnetic Recording).

 

Regards

0 Kudos
Reply