Please help about Timer interrupt of MPC5554

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Please help about Timer interrupt of MPC5554

ソリューションへジャンプ
2,710件の閲覧回数
quy1001
Contributor I

Hi members:

 

I am a beginer with MPC5554 processor.

Anybody please send me some example source code (or project folder) for using Timer Interrupt of MPC5554 in C. 

 

Thank you very much.

 

Sincerely,

Le Ngoc Quy.



Message Edited by quy1001 on 2008-01-20 01:23 PM

Message Edited by quy1001 on 2008-01-20 01:23 PM
タグ(1)
0 件の賞賛
返信
1 解決策
1,368件の閲覧回数
n_
Contributor II
Hi,
You must install CodeWarrior for MPC55xx, you can download it in Freescale.
In the Installed folder find the examples at: (CodeWarrior_Examples)\PowerPC_EABI\555x_Cookbook.
Example of Timer interrupt is FIT(Fixed Interval Timer) and DEC(Decrementer).
Regards,
Nguyen

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,369件の閲覧回数
n_
Contributor II
Hi,
You must install CodeWarrior for MPC55xx, you can download it in Freescale.
In the Installed folder find the examples at: (CodeWarrior_Examples)\PowerPC_EABI\555x_Cookbook.
Example of Timer interrupt is FIT(Fixed Interval Timer) and DEC(Decrementer).
Regards,
Nguyen
0 件の賞賛
返信