Pin connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pin connection

1,061 Views
Amiliy
Contributor I

Part:TDA8932BTW/N2,118 ,Is it normal that pins 1, 16, 17 and 32 are not connected by X-ray? Please help to give an explanation, thanks!TDA8932BTWN2,118.png

0 Kudos
Reply
4 Replies

1,010 Views
Wilma
Contributor I

A pin joint is a connection between two objects that allows only relative rotation about a single axis. All translations as well as rotations about any other axis are prevented — the joint therefore has one degree of freedom (1-DOF).

rapidfs.com

0 Kudos
Reply

1,015 Views
guoweisun
NXP TechSupport
NXP TechSupport

Are these 1, 16, 17 and 32pins  electric connected together when you test this part?

0 Kudos
Reply

999 Views
Amiliy
Contributor I

Only 1 pin is connected, 16,17,32 are not connected

0 Kudos
Reply

988 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please see X-RAY picture attached.

0 Kudos
Reply