PTN5150 VCONN /Accessory detect in UFP mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTN5150 VCONN /Accessory detect in UFP mode

Jump to solution
1,265 Views
IO_652434
Contributor II

What does PTN5150 expect to see on the USB side (CC pins) to detect the following modes?

  1. Analog Audio Accessory
  2. Debug Accessory
  3. VCONN cable

We are running in UFP mode and may not have the DFP/ charger on the other end of accessory or cable. Is it still possible to detect one of the above accessories if it is plugged by itself into UFP?

Tags (1)
0 Kudos
1 Solution
1,233 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Igor,

yes, that is correct. I would recommend you to purchase OM13584 PTN5150A-PTN36043 USB Type-C CC Logic Evaluation Kit

With Best Regards,

Jozef

View solution in original post

0 Kudos
4 Replies
1,250 Views
IO_652434
Contributor II

So would I need to bounce between UFP and DFP modes or stay in DRP if I want to be able to charge in one

case and detect accessory in another?

0 Kudos
1,234 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Igor,

yes, that is correct. I would recommend you to purchase OM13584 PTN5150A-PTN36043 USB Type-C CC Logic Evaluation Kit

With Best Regards,

Jozef

0 Kudos
1,194 Views
IO_652434
Contributor II

Tested with EVK and if I leave it in DRP mode it pulses CC ins and detects DFP and UFP nicely. Thanks!

0 Kudos
1,256 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Igor,

if the PTN5150 is working only in UFP (Upstream Facing Port), the CC1 and CC2 are connected through the internal pull-down resistors to the GND.

JozefKozon_0-1646993610599.png

Port exclusively consumes power. The CC1 and CC2 can detect only the voltage sources in the UFP configuration, it cannot detect a connection of any cable without a voltage source. 

With Best Regards,

Jozef

 

0 Kudos