PTN3460 resolutions in single LVDS bus mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PTN3460 resolutions in single LVDS bus mode

516 Views
norton
Contributor II

PTN3460:

What is the max resolution for single LVDS bus mode?

0 Kudos
1 Reply

409 Views
lisettelozano
NXP Employee
NXP Employee

Hello Michael,

Please accept my apologies for the delayed response.

PTN3460 single LVDS bus supports up to 112 MHz pixel clock, so PTN3460 can support any resolution as long as it is required less than 112 MHz pixel clock. The resolution supported is up to 1280x1024 @ 60Hz.

We do provide some VESA standard resolution table (10.1 Display resolution) in PTN3356 datasheet that you can refer to it, or you can go to VESA website (www.vesa.org) to download complete VESA timing list (need VESA member to be able to download it).

I hope this can be helpful.

Have a great day,

Paulina

0 Kudos