PN7462 with bluetooth module

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PN7462 with bluetooth module

675 Views
kralsemo06
Contributor I

Hi everyone,

We have a project the PN7462. This device can be connected to the computer interface and work as a mobile at the same time. We can't use USB and Uart at the same time because of the HIF module(In this case the compiler doesn't allow it). We use it for LCD with full SPI interface. We solved it using I2C to Uart converter. We communicate with the bluetooth module over UART.

 

Can u suggest a bluetooth module for these functions,

 

Best regardas,

0 Kudos
Reply
1 Reply

663 Views
fangfang
NXP TechSupport
NXP TechSupport

Hi @kralsemo06 ,

>> We communicate with the bluetooth module over UART. Can u suggest a bluetooth module for these functions
What's the function of the bluetooth module expect to UART interface? Eg. Audio transfer or command to control simple device like switch or light?
If Audio. Please refer to the IW416 EVK board as the link.
URL:https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth/aw-am510-evaluation-board:AW-AM510-USD
If switch or light control. Please refer to the QN9090 module as the link.
URL:https://www.nxp.com/products/wireless/bluetooth-low-energy/qn9090dk-development-platform-for-qn9090-....

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply