PN7462 with bluetooth module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PN7462 with bluetooth module

649 次查看
kralsemo06
Contributor I

Hi everyone,

We have a project the PN7462. This device can be connected to the computer interface and work as a mobile at the same time. We can't use USB and Uart at the same time because of the HIF module(In this case the compiler doesn't allow it). We use it for LCD with full SPI interface. We solved it using I2C to Uart converter. We communicate with the bluetooth module over UART.

 

Can u suggest a bluetooth module for these functions,

 

Best regardas,

0 项奖励
回复
1 回复

637 次查看
fangfang
NXP TechSupport
NXP TechSupport

Hi @kralsemo06 ,

>> We communicate with the bluetooth module over UART. Can u suggest a bluetooth module for these functions
What's the function of the bluetooth module expect to UART interface? Eg. Audio transfer or command to control simple device like switch or light?
If Audio. Please refer to the IW416 EVK board as the link.
URL:https://www.nxp.com/products/wireless/wi-fi-plus-bluetooth/aw-am510-evaluation-board:AW-AM510-USD
If switch or light control. Please refer to the QN9090 module as the link.
URL:https://www.nxp.com/products/wireless/bluetooth-low-energy/qn9090dk-development-platform-for-qn9090-....

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 项奖励
回复