Hi All,
Greetings
I am trying to interface PN5190 NFC Reader with another host controller. I am using the discovery loop example provided by the library. I am having doubts in the configuration of IRQ and its uses. I have used the following configuration
IRQ pin at host controller - GPIO External Interrupt with rising edge detection and pull down configuration.
please confirm if this is correct.
Can someone in the community please clarify how this interrupt is triggered how the values are changed wrt irq pin. I am not having a clear idea in the values of irq pin when a command is being sent to the pn5190.
please clarify on this aspect.
Thanks for your support.
PSJ
Hi PSJ:
You can refer to function phhalHw_Pn5190_WaitIrq() for more details. The function is waiting for the event E_PH_OSAL_EVT_RF, it should be posted by CLIF ISR once the interrupt line goes high to the CLIF HAL. The timeout value is 10s.
please also refer to the data sheet for IRQ pin.
Regards
Daniel
Hi @danielchen
Greetings
Thanks for your reply
Actually we are now able to detect for some types of RFID tags and Bank Cards as shown in the figure
The UID SAK and Type have been printed. But we have some issues.
1.This detection is happening only once, the discovery loop is running continously and from the second time onwards the discovery loop is not able to detect the technology type and going into stuck state.
2. We have an EMV Maestro test card with which we are not able to detect the cards on the discovery loop. While adding some print statements we are found that the function "wDiscloopStatus = phacDiscLoop_Sw_Int_PollMode(pDataParams); " returns the value 16523 while a card is detected and when this particular mentioned card is presented then value 16518 is returned. please refer to the print values observed.
Kindly suggest solutions for this particular issues.
Thanks for your support
Philip
Hi @pyt351
The discovery loop should detect your cards if you remove the card from the RF field and then move back to it again. The Ex1_DiscoveryLoop demo in the reader library can run very well. I would suggest you refer to this demo.
Regards
Daniel