PN5180 has a die identifier.
What is different about the die if the die identifier is different?
for example,
The size of the die.
Bonding wire routing.
The on-resistance of the TX part.
etc.
Best regards,
Hello @Shio_Tamba
die identifier : Each die has a unique Identifier. This entry can be treated as 16 byte unique random number.
That's means unique chip serial number. So there is the different die identifier is different unique chip serial number.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hi,
I would like to know the difference in physical characteristics between different die identifiers.
Best regards,
Hello @Shio_Tamba ,
Thanks for your update information.
There is not the difference in physical characteristics.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------