Recommended value:
master : C = 1nF;
Slave : C = 220pF
if I change the capacitance value to :
master : C = 220pF;
Slave : C = 1nF
What effect would that have?
Solved! Go to Solution.
if no filter on lin pin?
Thanks a lot~
What if I change it to any other value? Whether is also affect EMI?
Yes,the value of Cmast and C slave are calculated to define,so please don't suggest to change it!
The customer wants to replace friend business with NXP.
master:C = 220pF
They don't want to change the peripheral loop ,they want to replace it directly.
Does the number of slave nodes matter if the master C is reduced?
It will affect on the EMI/C performance.