PCF8566

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCF8566

696件の閲覧回数
ben_redmon
Contributor I

I am looking for a specification for the expected frequency min/max of the built-in internal oscillator (fosc) of the PCF8566 LCD Driver IC. The spec sheet only lists a range for fclk, which can be externally supplied or set to be fosc, as ranging from 125kHz to 315kHz. Does this mean that the internal oscillator (fosc) can have such a wide range of possible frequencies?

タグ(1)
0 件の賞賛
返信
1 返信

650件の閲覧回数
guoweisun
NXP TechSupport
NXP TechSupport

Hi

Yes,the internal oscillator (fosc) can have such a wide range of possible frequencies!

0 件の賞賛
返信