PCF2129 time errors

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCF2129 time errors

7,095 Views
juliancox
Contributor V

I am using a PCF2129 with a S08QE micro controller communicating via I2C. The circuit is exactly the same as the example in the data sheet and application note. Battery backup is supplied by a 3V button cell. All settings ar default values and the only initialisation is to clear any interrupt flags (writing 00 to Control Register 2). Software is created using Codewarrior V11.1 and communication is achieved through the I2C component of ProcessorExpert at 400Khz. We have 20 samples and everything works correctly - The controller can read and display the time, which can set via application software.

When the systems are powered up some of the units display the wrong time. The number of "faulty" units varies between 3 and 8 and they are NOT the same units each time and the "actual incorrect times" also varies each time. The batteries are all new. After the incorrect time is corrected the units all function correctly until the power is re-cycled (MAYBE!!!!!).

0 Kudos
Reply
17 Replies

6,770 Views
juliancox
Contributor V

I am getting rather despondent. We still have between 10% and 20% of devices losing time between power off and power on. I have tried every one of your suggestions - but to no avail. We monitored the alarm registers. We made a note of the contents of the alarm registers, switched off, waited about one hour and switched on. Of those that showed the wrong time we checked the alarm registers - they were all correct. 

0 Kudos
Reply

6,765 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Julian,

I see you have posted another question a week ago, but in my PC it was updated only now with your second message. I didn't see your first message a week ago. I apologize for that, its a system issue. I don't have any other idea what could cause the time lose. I have contacted an application engineer dealing with RTCs for an advice. As soon as I will receive an answer from him I will definitely reply to you.

Thank you for your patience.

With Best Regards,

Jozef

0 Kudos
Reply

6,700 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Julian,

I still haven't received an answer from the application engineer. As soon as I will receive an answer from him I will definitely reply to you.

Thank you for your patience.

With Best Regards,

Jozef

0 Kudos
Reply

6,680 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Julian,

I have checked your schematic again and I am missing the bulk capacitor on the VDD pin. Please refer to the Figure 48. in the PCF2129 datasheet. Because the direct switch to battery helped to diminish the issue, I suspect that without the 6.8uF bulk capacitor the internal operating voltage drops too low causing the oscillator to stop temporarily in some cases. Please try to add the 6.8uF capacitor on the VDD pin, which might hold the internal operating voltage at proper value during the battery switching.

JozefKozon_0-1650964599948.png

With Best Regards,

Jozef

0 Kudos
Reply

6,665 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Julian,

I apologize for sending you another update. I am reading an AN11186, because of another case, and in section 5.3 an RC network on the VDD pin is recommended. Please check it an if the 6.8uF bulk capacitor doesn't help, please try to add the 330Ohm resistor.

JozefKozon_0-1651049006687.png

With Best Regards,

Jozef

 

0 Kudos
Reply

6,860 Views
juliancox
Contributor V

Latest update.

Of the 20 units on test - 2 lost time (let us assume for the purpose of this report that it was one hour late). This time we did not correct the time, but carried on with the power cycling test. They continued displaying the "correct" time, but one hour late. With a production of several thousand units this is still a problem.

0 Kudos
Reply

7,092 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Julian,

I presume the time error occurs on the devices where the battery switch happens second time. Please refer to section 8.11.4 and Table 71. in the PCF2129 datasheet. If the battery switch occurs for the first time, the time and date are stored in the timestamp registers, because the BF bit in the Control_3 register is set to 0 by default, but after the battery switch occurs, the BF bit is set to logic 1 and in the next battery switch the timestamp registers are not modified.

Please set the BF bit to logic 0 after the battery switch occurs. This should solve the issue with time errors. 

JozefKozon_0-1648192153893.png

Please also check this example code from Tomas in this link

With Best Regards,

Jozef

0 Kudos
Reply

7,086 Views
juliancox
Contributor V

THank you for this information. I have not yet had an opportunity to test it, but I hope you can explain something.

I understand what the timestamp registers are for, but how does this affect the contents of the time registers. Why should they change when all the timestamp registers do is to record the time at which an event occurred?

0 Kudos
Reply

7,051 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Julian,

you are right. I posted my answer too hastily. The timestamp registers will most probably not affect the time registers. Could you please check the section 8.8.8 in the PCF2129 datasheet? Could you please confirm, that the all accesses are completed within one second? Also is the reading access made in one go? 

JozefKozon_1-1648450891968.pngJozefKozon_2-1648450939301.png

Could you please test the Tomas's code and see if it solves the issue?

With Best Regards,

Jozef

0 Kudos
Reply

7,046 Views
juliancox
Contributor V

All accesses are made in one go. I only read seconds, minutes and hours and I do not use the seconds information, but I read the time every half second.This is not really necessary - i just make use of an existing timing loop - which I can easyily extend.. Also it would appear that the consequence of section 8.8.8 are a roll-over whereas my problem can show difference of several hours. To illustrate this - in one example at 08:00 the units were switched on and one unis showed 15:27

0 Kudos
Reply

7,033 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Julian,

The functionality of the battery switch-over is limited by the fact that the power supply VDD is monitored every 1 ms in order to save power consumption. Considering that the battery switch-over threshold value (Vth(sw)bat) is typically 2.5 V, the power management operating limit (VDD(min)) is 1.8 V and that VDD is monitored every 1 ms, the battery switch-over works properly in cases where VDD falls with a rate lower than 0.7 V/ms. Could you please provide oscilloscope waveform of VDD, VBAT and CLKOUT during the VDD switchover event?

What are the settings for COF[2:0] and PWRMNG[2:0] bits? 

Please share your schematic with voltage levels and part values.

With Best Regards,

Jozef

0 Kudos
Reply

7,012 Views
juliancox
Contributor V

COF[2:0] is 000 (default)

PWRMNG[2:0]] is 000 (default)

Waveform A shows the initial voltage drop which is 0.64V in 40ms giving a rate of 16mV/ms. The display is 100mv/cm and 10ms/cm

Waveform B shows the whole supply voltage decay. The display is 0.5V/cm and 500ms/cm.

The discontinuity (shown clearer in waveform A) can be attributed to the shutting down of the LED display (7 off 7-segment digits)

The battery voltage remains constant at 3.0V throughout.

Regarding the schematic, Vcc is 3.3V, V_Batt is 3.0V and R9 and R10 have been changed to 1K8

0 Kudos
Reply

6,998 Views
juliancox
Contributor V

SORRY, I forgot to mention, I cannot get any useful measurement from CLKOUT as it is an open drain and  nothing is connected to it.

 

0 Kudos
Reply

6,966 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Julian,

thank you for the schematic and the scopes. So the too high fall rate is not the reason. 16mV/ms is way lower, than 700mV/ms.

I have two suggestions. Please test them.  

1. Please disable the CLKOUT output by the COF[2:0] bits in the CLKOUT register, address 0Fh. This probably will not help, but please test it. 

JozefKozon_0-1648806918135.pngJozefKozon_1-1648806953338.png

2. This suggestion might solve your issue. How are set the PWRMNG [2:0] bits in the Control_3 register, address 02h? Are they left default? 

JozefKozon_2-1648807135421.png

Please set to bits to 011 to direct switching mode, so the internal operating voltage doesn't drop to Vth(sw)bat, but switches to VBAT supply when the  VDD < VBAT. 

JozefKozon_3-1648807191830.png

JozefKozon_4-1648807317412.pngJozefKozon_5-1648807352574.png

With Best Regards,

Jozef

0 Kudos
Reply

6,959 Views
juliancox
Contributor V

Thank you for the suggestions - I will try them. I have been reluctant to try the Direct Mode because VDD is 3.3V and VBATT is 3.0V.

0 Kudos
Reply

6,913 Views
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Julian,

ok. Hopefully it will solve the issue.

With Best Regards,

Jozef

0 Kudos
Reply

6,644 Views
juliancox
Contributor V

I am starting to get somewhat despondent. We have tried all recommendations and we are still getting approximately 10% failures. I am fairly convinced that the time registers are being corrupted when the unit is switched off. The unit is a time and temperature controlled (hence the clock chip) 150W heater. The heater is switched by the micro controller via a zero-crossing OPTO coupler and a TRIAC. We are testing 20 110V units - all fed from a local 220/110V transformer, but we don't know if the interference is caused on the board  or via the transformer. the random factors are: -

When power is removed from the board, is the heater ON , OFF or switching?

When power is removed from the board, is the I2C in the process of transferring data?

0 Kudos
Reply