PCA9546A I2C MUX Bus Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCA9546A I2C MUX Bus Problem

511 Views
berntau
Contributor I

Hi,

I designed this into a new product or ours.

I notice that the chip frequently results in an I2C bus stuck event that needs recovery.

This occurs when writing the control register for a MUX selection, followed immediately bu a read to confirm the correct selection.

The bus will sometimes become stuck in that SDA remains low forever or until bus recovery procedure.

The bus become stuck at around bit 8 or Ack of read data address. See attached wave capture.

This happens at a frequency of around 1 in 1000 or in my case about every 3 minutes.

Bus operation is 100kHz.

What can cause this problem?

The bus signals are clear and beautiful. Is there a minimum time specification between a write followed by read ?

I cannot see it in the datasheet.

Regards

Bernt

0 Kudos
Reply
0 Replies