P3S0200可以工作在1.8V的IIC上吗

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P3S0200可以工作在1.8V的IIC上吗

248件の閲覧回数
赵中飞
Contributor I

P3S0200的VCC我用3.3V,IIC我用1.8V可以吗

0 件の賞賛
返信
1 返信

239件の閲覧回数
JozefKozon
NXP TechSupport
NXP TechSupport

Dear Zhao,

please refer to the Table 7. in the P3S0200 datasheet. The VCC voltage sets the VIH and VIL levels for the input pins. If VCC=3.3V, than minimum voltage required on the input pins, to be recognized as logic high it 0.46*VCC=0.46*3.3V=1.518V. You can use the 1.8V for the input pins. The 1.8V will be recognized as logic high.

JozefKozon_0-1700481975929.png

 

With Best Regards,

Jozef

0 件の賞賛
返信