OTA Update from IOS for MKW31Z512

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

OTA Update from IOS for MKW31Z512

450件の閲覧回数
christopher_den
Contributor I

Dear NXP,

My team and I are working on a project using MKW31Z512 w/BLE. We are trying implement OTA transfer of .srec file from an IOS mobile application we built. Are there any code examples or guides available for IOS developers to implement OTAP in mobile application for this chip?

thanks.

タグ(2)
0 件の賞賛
1 返信

410件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Chris, I hope you're doing well!

 

There's an example project available in the KW31Z/KW41Z's SDK showing how to configure the device and perform an OTA update from either the iOS or Android IoT Toolbox mobile applications to the KW31Z/41Z.

 

This SDK example can be found on the following path of the KW31Z's SDK:

<…\SDK_2.2.1_MKW31Z512xxx4\boards\frdmkw41z\wireless_examples\bluetooth\otap_client_att>

 

There's also more information about the OTA procedue in the BLE Application Developer's Guide, in the following path of the SDK:

<…SDK_2.2.1_MKW31Z512xxx4\docs\wireless\Bluetooth\BLE Demo Applications User's Guide.pdf>

 

For development purposes, we recommend using the FRDM-KW41Z even if development is being done for the KW31Z. These devices are compatible as long as the code doesn't use components not found on the KW31Z version of the MCU.

 

Please let me know if you need any more information.

 

Best regards,

Sebastian

0 件の賞賛