NXQ1TXH5 application

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXQ1TXH5 application

628 Views
549290520
Contributor I

Dear all.

      When I look at the NXQ1TXH5 data sheet, I don't understand the functions of pins 3 and 4 (SDA and SCL). If I don't use these 2 pins, can I implement the wireless charging function?Thanks

0 Kudos
Reply
1 Reply

519 Views
lisettelozano
NXP Employee
NXP Employee

Hello Hualong,

Yes, you can still implement the wireless charging functions if you don’t use these 2 pins.

The pins 3 and 4 (SDA and SCL) are for the I2C interface as part of the support interface for the NXQ1TXH5.

The NXQ1TXH5 is an easy to use fully integrated chip that can be completely configured by means of external resistors so in general there is no need for customers to have access to the I2C bus to configure the chip.

You can check section 2.1.7 Support interface for the application note AN11775 https://www.nxp.com/docs/en/application-note/AN11775.pdf

Have a great day,

Paulina

0 Kudos
Reply