Hello,
We are planning to apply NFC Reader IC PN7150 to other vendor's MCU instead of NXPs'
OS is RTOS.
Do we have to use a specific MCU in order to communicate between PN7150 and MCU through NCI protocol?
or Is it possible to integrate NXP-NCI to other vendor's MCU through SW porting?
I wonder if NXP_NCI can be implemented to other vendor's MCU as well regardless NXP products.
Thank you,
Best regards,
Andy
已解决! 转到解答。
Hello,
Yes. the application is OK. But The porting to other MCUs is not supported by NXP. Fortunately, you can refer to AN11990 and to the software examples available for our MCUs in the software examples which you can take as reference for your project
URL:https://www.nxp.com/docs/en/application-note/AN11990.pdf.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hello,
Yes. the application is OK. But The porting to other MCUs is not supported by NXP. Fortunately, you can refer to AN11990 and to the software examples available for our MCUs in the software examples which you can take as reference for your project
URL:https://www.nxp.com/docs/en/application-note/AN11990.pdf.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------