NHS3152 I2D Offseet Current settings

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NHS3152 I2D Offseet Current settings

715 次查看
bmeyer
Contributor II

Hello NXP:

When setting up the I2D converter, there are two I offset settings but no description as to magnitude or sign. Plus no explanation of how these are used.

0 项奖励
3 回复数

639 次查看
driesmoors
NXP Employee
NXP Employee

Hello @bmeyer

Did you have a look at the firmware documentation?

Check <SDK>/docs/firmware.html > Documentation of the low-level HW block drivers > i2d: Current to Digital converter driver

 

Kind regards,
Dries

0 项奖励

701 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @bmeyer ,

 

Unfortunately there is no detailed documentation available for the I2D block. but if you are willing to share the expected current range and an electrical model of the current source, we can assist you setting up the system.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励

681 次查看
bmeyer
Contributor II

Hello Kan:

Thanks for the reply. I'm not sure what I could share. I'm trying to figure out how the I2D system works on the NHS3152 IC. Although, settings without sufficient explanation make understanding difficult. 

0 项奖励