Hello NXP:
When setting up the I2D converter, there are two I offset settings but no description as to magnitude or sign. Plus no explanation of how these are used.
Hello @bmeyer
Did you have a look at the firmware documentation?
Check <SDK>/docs/firmware.html > Documentation of the low-level HW block drivers > i2d: Current to Digital converter driver
Kind regards,
Dries
Hello @bmeyer ,
Unfortunately there is no detailed documentation available for the I2D block. but if you are willing to share the expected current range and an electrical model of the current source, we can assist you setting up the system.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello Kan:
Thanks for the reply. I'm not sure what I could share. I'm trying to figure out how the I2D system works on the NHS3152 IC. Although, settings without sufficient explanation make understanding difficult.