NCX2200 for 105°C

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NCX2200 for 105°C

594 Views
malma
Contributor I

I want to use the NCX2200 for up to 105°C. Which electrical conditions do change significant?

Maybe you can give me a modified datasheet?

Regards

M.Malsam

0 Kudos
Reply
1 Reply

522 Views
diegoadrian
NXP Employee
NXP Employee

Hello Markus,

 

Thank you for writing.

 

I really apologize, but unfortunately, we do not have that type of information.

 

Furthermore, we do not recommend you use the NCX2200 above the recommended operating conditions. This may cause variations in the output or a permanent damage to the device.

 

Best regards,

Diego.

0 Kudos
Reply