Multi-Protocols RFID Reader

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi-Protocols RFID Reader

1,055 次查看
shai_b
Senior Contributor II

Hello Team,

My Customer is looking for RFID Reader, suitable for an outdoor device.
Could you please advise if NXP platform can support reading for the following tags:
HID iCLASS®
HID iCLASS® Seos®
HID Prox 125 kHz
HID Indala 125 kHz
SE credentials (iCLASS SE/Elite, MIFARE SE, DESFire EV1 SE...)
MIFARE® Classic / Ultralight /DESFire EV1...
NFC Tags Reader/Writer mode3

waiting for your kind responses, Thanks.

Best regards,

Shai 

标记 (4)
0 项奖励
回复
3 回复数

1,034 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

We have this HITAG reader available, still, the support of this is limited and not recommended for new designs.

Still, you can check with one of the companies in the RFID ecosystem as there are several consultants and system integrator that might have some multi-frequency readers.

 

Hope this helps,

 

 

Regards,

Estephania

0 项奖励
回复

1,047 次查看
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

I apologize for the inconveniences this might cause you, but we do not have a single reader that supports all the requirements in your list.

You can find in this list the available reader we have for NFC.

 

Still, you can check with one of the companies in the RFID ecosystem as there are several consultants and system integrator that might have some multi-frequency readers.

 

Hope this helps,

 

 

Regards,

Estephania

0 项奖励
回复

1,041 次查看
shai_b
Senior Contributor II

@estephania_mart hello,

Thank you for your response, So if I understand correctly NXP doesn't have any 125khz RFID reader only a 13.56Mhz (NFC) reader such as PN5180 but without any support of any LF band?

Does NXP plan to release such an LF RFID reader any time in the future?

Thanks and Regards,

Shai 

0 项奖励
回复