Hello,
i'm using 20XS4200 dual switch to drive a motor load or a Bulb load. i want to implement the auto-retry feature in order to protect my HW.
according to reference manual of the 20XS4200 circuit to activate the Auto-retry feature i need to update the retry_s bit in the RETRYR register with the correct value according to CONF[x] pin.
the behavior i got is that the auto retry works only with bulb load.
Used Configuration is:
- retry_s set to 0 when CONF = 0 ==> Bulb Load ==> Auto retry works fine
- retry_s set to 1 when CONF = 1 ==> Motor Load ==> Auto retry do not work, the output is turned down for good from the first time.
any help would be appreciated. thanks in advance.