Hi sir,
From the document MV-S302681-00 (Application note – wake on wireless) ,
WOW can be configured by setting mef.conf, we have tried it but cannot wake up the host.
Is there any documents about how to config mef.conf?
If we config mef.conf and also use "hscfg" command, how is the procedure and which one has higher priority on setting WOW?
Thank you.
Hello @frank8888
After driver building is done in wlan_src, a bin_wlan directory is created , which is located at the same level as that of wlan_src. see below, please!
in it, you will found mef.conf
Have a good day!
Regards,
weidong
Hi Weidong,
Thanks. We would like to know how to config this mef.conf file for WOW.
Is there any document for reference?
Can we use only this config file for WOW, or we need also to set with "uaputl hscfg 0x4f 0xff 200" command?
Thank you.
Hi @frank8888 ,
1. PIN PCIE_WAKEn
I checked datasheet of 88W9098
It requires external pull up. can you check it? The pin is fixed for wifi wake host.
2. reference
what I gave you in another post is our test steps for 9098 & 8997. The wifi card is M.2 KEY E interface.
See pin 55 of M.2
Test steps:
1. modprobe moal mod_para=nxp/wifi_mod_para.conf
2. wpa_passphrase NETGEAR15-5G boldmango026 >> /etc/wpa_supplicant_5g.conf
3. wpa_supplicant -B -i mlan0 -c /etc/wpa_supplicant_5g.conf -D nl80211
4. udhcpc -i mlan0
5. iw phy#0 wowlan enable any
6. cd /usr/share/nxp_wireless
7. ./mlanutl mlan0 hssetpara 2 0xff 0xc8 3 400 # NXP WiFi take PCIe M.2 wakeup gpio as PCIe in band
wakeup, since the gpio is PCIe specific pin.
8. Connect a test laptop to same AP with same local network
9. Check connectivity to DUT from test laptop, and vice versa
10. echo mem > /sys/power/state
11. Ping to DUT from test laptop to wakeup IMX
So above steps is enough.
Regards,
weidong