Hello,
I'm facing issues in executing flex spi nor polling transfer example using SPT tool (authenticated HAB) I'm using.
But debugging it works fine.
Please check this issue.
I'm using
(MXRT1020 , SDK_2_15_000_EVK-MIMXRT1020 , MCUXpresso IDE v11.9.1_2170, MCUXpresso Secure Provisioning v8)
Shealtiel Elizer
Could you provide more specific details on the issue you are having?
Best regards,
Omar
Wanted to flash FLEX SPI example code using authenticated HAB (SPT TOOL), it was written successfully but my code was not running after I switched it into boot mood.
Please refer to AN12681, there you can find detailed steps to use HAB. It may be possible that HAB is not well implemented so the image is not executed when flashing.
Best regards,
Omar