I would like to know if is there any proper guide for using FreeMaster for MWPR1516 LDO board calibration. I tried with the LDO board user guide but it's not working. Furthermore, I have multiple boards in my possession, and I'm wondering if it is necessary to calibrate each one individually. Is it possible to perform PGA and ADC calibration programmatically instead? Currently, I am utilizing the demo project specified in the MWPR1516 LDO user guide.
Thanks in advance
Dear Prabhath,
please refer to the following community thread from Jan.
https://community.nxp.com/t5/FreeMASTER/WPR1500-BUCK-with-FREEMASTER/m-p/1065751#M262
The software also supports the LDO board. You just need to change a macro definition in MWPR1516_config.h library. Please refer to the section 6.2.4 in WPR1500LDOMPUG attached.
With Best Regards,
Jozef