Hello,
Is there a solution to accelerate the spi flash read and write?
Because it's very long when I have to burn all the flash (around 30 min with the verification 15 min without it).
I use the spi_generic driver and my code looks like the spi_flash demo.
Jimmy
Hello Jimmy,
What is the size of the image you're burning to flash?
In addition to the C code demo, the Freescale CodeWarrior IDE also has the ability to burn the flash from the drop down menu. If you go to the Help -> Search drop down menu in CodeWarrior, and search for "Flash Programmer", you will find documentation on using this. I can't say this will be faster than the C project, but it is an alternative available.
Regards,
-Andrew
Hello,
I try to burn all the flash (64 Mbyte), it's for a test.
Jimmy