MRF300 simulation model

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MRF300 simulation model

Jump to solution
1,758 Views
DF5FS
Contributor I

Hello,

I am currently a little puzzled with the ADS simulation model of the MRF300 device.

The datasheet specifies V_ds(on) to be 0.16 V at V_gs = 10 V and I_D = 1A

However, when I connect the model up to V_ds = 0.16 V and V_gs = 10 V, I only see I_D of around 0.75 A.

I tried this when expected power output did not match the datasheets values by around 3 dB.

Am I in error, or does the model not match the parameters as layed out in the datasheet? At the moment I am not confident I can trust the model.

Labels (1)
  • RF

0 Kudos
1 Solution
1,714 Views
LPP
NXP Employee
NXP Employee


1.
You can find some information about FET models in these publications.

https://core.ac.uk/download/pdf/17180215.pdf
http://epubs.surrey.ac.uk/805122/1/PID1256805-1.pdf
http://epubs.surrey.ac.uk/803447/1/6565_final.pdf

2.
The datasheet DC parameters can differ from those obtained by simulations on several reasons.

- datasheet specs provide typical values. The model parameters may be based on different device instances. Generally, most critical simulated parameters fit the specified min-max range.

- the model has been optimized to fit measured data within some characterization limits. The priority is given to fit measured RF performance. The values beyond the characterization limits are extrapolated.

- Apparently, MRF300AN model parameters has been characterized at VGS<4V. The model mis-predicts drain current at higher VGS value. You can see it on simulated IDS vs VGS plot. The drain current increases from VGS 0V to 4.5V. It decreases at VGS>5V and it doesn't reach maximum at VGS=10V. This is unexpected behavior - the drain current must increase vs gate voltage (excepting thermal self-heating effects).

LPP_0-1611051681107.png

 

Note. This mis-prediction doesn't affect simulation of MRF300AN in it's normal operating mode as class AB amplifier. Typical peak current in this mode is about 12A that doesn't require VGS more than 4V.

LPP_1-1611051748590.png

The last note. Self-heating effects are important when doing DC simulation. In practice, DC characterization can be performed in pulsed mode to remove the influence of self-heating. The same effect can be obtained in simulation if you set model parameter RTH=0. You can see the difference of IDS vs VDS curves from the previous chart.

LPP_0-1611052846072.png

 

 

Best Regards

Pavel

NXP TIC

 

 

View solution in original post

2 Replies
1,681 Views
DF5FS
Contributor I

Thank you for the comprehensive answer.

I have simulated the 13.56 MHz reference circuit and found the results to be similar to what is specified in the Datasheet.

A push-pull configuration seems to be a lot more effort to match correctly as I have never seen better efficiencies than 60% in my simulations as well as experimental setups.

 

Best regards

Frederik, DF5FS

0 Kudos
1,715 Views
LPP
NXP Employee
NXP Employee


1.
You can find some information about FET models in these publications.

https://core.ac.uk/download/pdf/17180215.pdf
http://epubs.surrey.ac.uk/805122/1/PID1256805-1.pdf
http://epubs.surrey.ac.uk/803447/1/6565_final.pdf

2.
The datasheet DC parameters can differ from those obtained by simulations on several reasons.

- datasheet specs provide typical values. The model parameters may be based on different device instances. Generally, most critical simulated parameters fit the specified min-max range.

- the model has been optimized to fit measured data within some characterization limits. The priority is given to fit measured RF performance. The values beyond the characterization limits are extrapolated.

- Apparently, MRF300AN model parameters has been characterized at VGS<4V. The model mis-predicts drain current at higher VGS value. You can see it on simulated IDS vs VGS plot. The drain current increases from VGS 0V to 4.5V. It decreases at VGS>5V and it doesn't reach maximum at VGS=10V. This is unexpected behavior - the drain current must increase vs gate voltage (excepting thermal self-heating effects).

LPP_0-1611051681107.png

 

Note. This mis-prediction doesn't affect simulation of MRF300AN in it's normal operating mode as class AB amplifier. Typical peak current in this mode is about 12A that doesn't require VGS more than 4V.

LPP_1-1611051748590.png

The last note. Self-heating effects are important when doing DC simulation. In practice, DC characterization can be performed in pulsed mode to remove the influence of self-heating. The same effect can be obtained in simulation if you set model parameter RTH=0. You can see the difference of IDS vs VDS curves from the previous chart.

LPP_0-1611052846072.png

 

 

Best Regards

Pavel

NXP TIC