MMZ09332BT1 usage for 915MHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MMZ09332BT1 usage for 915MHz

670件の閲覧回数
msohani
Contributor I

The datasheet for MMZ09332BT1 shows a few test circuits for specific frequency ranges. I am planning to use this power amp for 915MHz, which is not included in any of the test circuits. How can the external components be selected to optimize for 915MHz?

ラベル(1)
  • RF

0 件の賞賛
返信
1 返信

581件の閲覧回数
andrei_skok
NXP Employee
NXP Employee
We offer the MMZ09332BT1 evaluation boards for the following frequency ranges:
136-174 MHz
400-500 MHz
717-768 MHz
860-875 MHz
900-930 MHz
925-960 MHz
Please contact your local NXP distributor to order the boards.


Have a great day,
Andrei

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信