MCIMX8QXP with MX8-DSI-OLED1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCIMX8QXP with MX8-DSI-OLED1

997 Views
thanhcn87
Contributor I

Hello,

I  have using i.MX 8QuadXPlus MEK run with Android P9.0.0_2.1.0_AUTO_GA_SOURCE.

When I used HDMI, Android can show on the screen.

But i used MX8-DSI-OLED1 touchscreen instead HDMI. No content to show.

Q: How can i setup to use MX8-DSI-OLED1?

IMG_20190514_171219.jpg

Thank.

Tags (2)
0 Kudos
Reply
1 Reply

831 Views
jamesbone
NXP TechSupport
NXP TechSupport

Hi,

Unfortunately in Android P9 there is no support for the MX8-DSI-OLED1,  if you like to test the MX8-DSI-OLED1,  you need to use Linux BSP and change the  Device tree,  fsl-imx8qm-mek-dsi-rm67191.dtb  it is the device tree that allows the usage of the DSI-OLED display.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply