Hello,
I have using i.MX 8QuadXPlus MEK run with Android P9.0.0_2.1.0_AUTO_GA_SOURCE.
When I used HDMI, Android can show on the screen.
But i used MX8-DSI-OLED1 touchscreen instead HDMI. No content to show.
Q: How can i setup to use MX8-DSI-OLED1?
Thank.
Hi,
Unfortunately in Android P9 there is no support for the MX8-DSI-OLED1, if you like to test the MX8-DSI-OLED1, you need to use Linux BSP and change the Device tree, fsl-imx8qm-mek-dsi-rm67191.dtb it is the device tree that allows the usage of the DSI-OLED display.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------