Dears:
Issue description:
-two project A and B. developed with same MCU and SBC(FS8510)
-in order to enter normal mode from debug mode,need to send 6 times WD_SEED to FS_WD_ANSWER.
-But, the WD_SEED value is 0x5AB2 all the time in project A. the WD_SEED value changed every times in project B, for example 0xF3BA.
-WD config is 0xB20B and FS_STATE value is 0x2009 in both A and B project.
-why this WD_SEED is different?
Thanks
Ziv
HI
Two questions for you:
1: you select Challenger watchdog in both project,right?
2:The MCU send the seed of the LFSR in both projects,right?
after power on reset the default value of seed is 0x5AB2.