Hello, I wonder if it would be possible to use the PC2TPLEVB with USB dongle to read data from a MC33772 TPL board via the evaluation GUI. There is a note in the PC2TPLEVB documentation claiming this is possible with the MC33775 but there is no mention about compatibility of any other boards.
Thanks!
which board about MC33772B do you mean? do you have the full name of MC33772B board?
Hi, I have two boards, the FRDM33771BTPLEVB and tthe KIT33772CTPLEVB.
Thanks!
Thanks for your feedback! Seems can't support these boards which are old version.