Hello, NXP!
I have some problems with TPL communication between MC33771B(2ea) and MCU(S32K144) ( with MC33664).
my configuration of SPIs for interfacing MC33664's like below
-----------------------------------------------------------------------------------------------------------------------------
Master SPI Tx: 2Mbps / 40bits/frame / PCS : active low / Second Edge / MBS / Interrupt type
Slave SPI Rx : 40bits/frame / PCS : active low / Second Edge / MBS / Interrupt type
Core Clock 80MHz
Initial Fault Status( no change afterwards )
CID1(1st daisy chain) COM_STATUS error count 2 / FAULT1 0x0040 FAULT2 0x0000 FAULT3 0x0000
CID2(2nd daisy chain) COM_STATUS error count 2 / FAULT1 0x0040 FAULT2 0x0000 FAULT3 0x0000
----------------------------------------------------------------------------------------------------------------------------
I am using NXP's BCC driver.
I'm trying to read/write registers about 20 times each, every 200ms.
But sporadically receive CRC(many)/TagID(few)/RC(few) mismatch errors. (average 1 error per 2 minutes )
At which point I should look into first to resolve this issue ?
Many thanks for your support in advance.
Sungho
Solved! Go to Solution.
Hello Sungho,
the first think I would look at is the physical interface - e.g. SPI lines, TPL lines, contacts etc. Also it would be helpful to monitor SPI/TPL lines with logic analyzer. If everything is correct, then the code you are using should be checked.
Regards,
Jakub
Hello Sungho,
the first think I would look at is the physical interface - e.g. SPI lines, TPL lines, contacts etc. Also it would be helpful to monitor SPI/TPL lines with logic analyzer. If everything is correct, then the code you are using should be checked.
Regards,
Jakub
Hi, thank you for your reply.
Me Resolved this issue by increasing priority of interrupt(SPI Slave/TPL).
Somehow losing synchronous read timing when there exist competitions with other ISRs(same priorities) especially in a burst read event (eg. 31 bytes raw value access)
Thanks,
See you