MC13224V Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC13224V Interrupt

1,260 Views
Epopeia
Contributor I

Hello,

I'm using MC13224V, and need to connect a detector zero-cross. This integrated circuit has no external interrupt. What should I do? I connect the keyboard (KBI)?
Thank you.

Francesco

Tags (1)
0 Kudos
Reply
2 Replies

671 Views
redbee
Contributor III

 


Epopeia wrote:

Hello,

I'm using MC13224V, and need to connect a detector zero-cross. This integrated circuit has no external interrupt. What should I do? I connect the keyboard (KBI)?
Thank you.

Francesco


KBI4-7 can be used to generate interrupts from external sources. I have some code in Contiki that does this. See http://mc1322x.devl.org for more details.
The ADCs can also be programmed to auto-run and generate interrupts at specific levels.
You can probably use the TMR modules for what you want too.
-Mar.

 

 

0 Kudos
Reply

671 Views
Epopeia
Contributor I

Mar,

 

Thank you.

0 Kudos
Reply