Hello, I was trying to install an the LTIB on Ubuntu 12.04. I have got through all of the package installs and changed the Ltibutils.pm to find the glibc-devel and zlib. I am stuck when running it errors with a host_config.log that contains only this:
rpmdb: --force-debian: unknown option
Died at ./ltib line 2337.
traceback:
main::setup_rpmdb:2337
main::check_rpm_setup:2400
main::host_checks:1423
main:542
Started: Tue Aug 7 11:15:31 2012
Ended: Tue Aug 7 11:15:31 2012
Elapsed: 0 seconds
Build Failed
Has anyone got LTIB on 12.04 running yet?
- I'm trying to get LTIB on 10.4, having problems
- so need to decide if 12.04 is a better way to go ...
This is for Sabre SDB, using L3.0.35_4.0.0_130424_images_MX6
Equally, is 13.04 a better way to go?
Thanks,
Phil
Good news!
- I got it to build ok on 10.4!
Before I tried the LTIB build, I did get the board booting into Ubuntu using the 'images' tar
- then LTIB build was the next logical step.
I'd now like to get it building under 12.04, as this is most likely a better platform going forward (since it's still supported)
- just to confirm, with BSP 4.0.0, no patches are necessary??
Hi Leo,
I am just wondering if I got right place to post my issue regarding not found the ssl/tls certificate on my ltib. I have litb bsp runs on imx6 target board. I have a qt app to send the mail to smtp.gmail.com using sslsocket. since smtp.gmail.com always uses ssl/tls certificate to verify the email received, so the send email failed during hand-shack, because the ltib does not have any ssl/tls certificates loaded.
So my question;
1) does ltib load ssl/tls certificates?
2) why I could not find the ssl/tls certificates and openssl.conf file?
3) do you have any information about the ssl/ltib certificate installation and generation for ltib?
Thanks,
-Bill Yang
Thanks Leo, I will post ssl/lts certificate question to a new discussion thread.
However, I had a building LTIB failure issue. I am tried re-build the LTIB BSP that was built in last year successfully, but now it failed as the error message below.
**** WARNING: Building without libstartup-notification
checking for EEL... configure: error: Package requirements (
gail >= 0.16
gconf-2.0 >= 1.1.11
gdk-pixbuf-2.0 >= 2
glib-2.0 >= 2.15.0
gio-2.0
gthread-2.0 >= 2.15.0
gtk+-2.0 >= 2.9.4
libglade-2.0 >= 2.0.0
libgnome-2.0 >= 2.23.0
libgnomeui-2.0 >= 2.7.92
gnome-desktop-2.0 >= 2.23.3
libxml-2.0 >= 2.4.7
) were not met:
No package 'gail' found
No package 'gconf-2.0' found
No package 'gdk-pixbuf-2.0' found
No package 'gtk+-2.0' found
No package 'libglade-2.0' found
No package 'libgnome-2.0' found
No package 'libgnomeui-2.0' found
No package 'gnome-desktop-2.0' found
Consider adjusting the PKG_CONFIG_PATH environment variable if you
installed software in a non-standard prefix.
Alternatively, you may set the environment variables EEL_CFLAGS
and EEL_LIBS to avoid the need to call pkg-config.
See the pkg-config man page for more details.
error: Bad exit status from /home/byang/ltib/tmp/rpm-tmp.12726 (%build)
I have no idea what the EEL error means. Can you help me to figure out this issue?
thanks,
-Bill
I too have been trying for days to get ltib to work.
I have tried Ubuntu 12.04, 10.04 and Fedora 12
The closest I got was Ubuntu 10.04, but the squashfs was not built.
What is the point of Open source if the sources don't build?
Why can't Freescale provide a VM with the tools correctly installed and working?
Hi Larry,
I sympathize!
However, I've just got the LTIB building under 10.4!
- see
These lines seemed to sort my issues out:
2) create a soft link under /usr/include.
sudo ln -s i386-linux-gun/sys sys
3) install additional packages.
sudo aptitude -y install asciidoc texlive-latex-base dblatex xutils-dev
sudo apt-get install texinfo
4) modify ltib/dist/lfs-5.1/base_libs/base_libs.spec.
...
perl -w -e '
# @ARGV = grep { `file $_` =~ m,ASCII C program text, } @ARGV;
# exit (0) unless @ARGV;
Hope that helps!
I will now try 12.04 ....
Hi William,
I do on 12.04.
Follow All Boards LTIB Config Ubuntu to setup unbutu.
Download this L3.0.35_4.0.0_ER_SOURCE to install ltib
Than L3.0.35_4.0.0_AACP_CODECS and L3.0.35_4.0.0_MM_CODECS ( to find under Middleware-Codecs and other Algorithms (4) )
Extract and copy the contend of the ltib codecs folder (do not extract) into the dpkg folder of the ltip installation.
Helpful is to have a look in L3.0.35_4.0.0_LINUX_DOCS but don't set up Ubuntu 9.04 did not realy work for me.
Do that what Eric says:
The answer seems to be simple. Go into ltib/dist/lfs/base_libs/base_libs.spec and find these lines:
# remove absolute paths from text search files (if they exist)
perl -w -e '
@ARGV = grep { `file $_` =~ m,ASCII C program text, } @ARGV;
exit(0) unless @ARGV;
Remove the last two (the lines beginning with "@ARGV" and "exit(0)" and you should be good to go.
By the first run the maybe some fault. It is helpful to copy that and use the search function here.
Joerg
Hi joergboge,
I follow your instruction to download L3.0.35_4.0.0_ER_SOURCE to install LTIB.
I have been successful to install it to Ubuntu 12.04.I run ./ltib -c and choose imx6q as the target board.I got succeeded.
But I can not compile the imx53_loco board.Because no linux-2.6.35 in this LTIB.
How can I run it.
Please help me.
regards!
william
Sorry, I never got round to trying on 12.04
- at the time I found VirtualBox v4.2.12 had a problem with ubuntu 12.04
- so, I stayed with 10.4
- I believe VirtualBox v4.2.14 fixes the ubuntu 12.04 problem
- but I have not gone back to it, as I seem to be ok on 10.4 at the moment
If I was you, I would try 10.4
- install all the upgrade packages
- also make sure you do steps 2) - 4) that I did above....
That may help you figure out the steps for 12.04 if you still need to go to that...
IIRCC, I did the standard 9.04 steps for 10.4, then when that failed, I did 2) - 4) above, and that got it going...
I assume that LTIB on Ubuntu 13.04 didn't work on 12.04 for you?